Library
search
close
en
  • Englishdone
  • Deutsch
  • Español
  • Français
  • Hrvatski
  • Italiano
  • Nederlands
  • Norsk
  • Polski
  • Português
  • Russian
  • Slovensky
  • Srpski
  • Suomi
  • Svenska
  • 汉语
RelevancyPublication datearrow_drop_upPublication datearrow_drop_down
English
cancel
Documents found: 189
PUBLIC
Tech Note 262: GFCI circuit breakers with ABB drives
ID:LVD-EOTKN262U-EN
,
REV:A
English
VFDs (AC drives) use high-frequency switching to control motor speed and torque. This switching can create common-mode (CM) noise and high-frequency leakage currents that may cause nuisance tripping when a conventional Class A GFCI is installed on the line supply power feeding a drive. This technical note explains the cause, outlines mitigation practices, and summarizes recent UL developments that recognize “HF” designed  Class A GFCIs evaluated for improved immunity to high-frequency differential current.
Application note
Application note
2026-08-06
PUBLIC
Tech Note 256: Fuse class substitutions for ACS380 drives
ID:LVD-EOTKN256U-EN
,
REV:A
English
This application note clarifies when Class CC fuses are acceptable for some ACS380 drives after a wording change in the latest Branch Circuit Protection document, (Rev K).
Application note
Application note
2026-06-22
PUBLIC
Tech Note 257: Installing VFDs on open-delta systems
ID:LVD-EOTKN257U-EN
,
REV:A
English
This Technical Note outlines practical techniques to improve performance for ABB low voltage VFDs supplied from open-delta transformers.
Application note
Application note
2026-06-22
PUBLIC
Tech Note 259: Control Word Sequences in ABB Drives Profile Communication
ID:LVD-EOTKN259U-EN
,
REV:A
English
When controlling all compatible ABB AC drives via fieldbus communications using the ABB Drives Profile, users often employ simplified control word sequences to start and stop the drive.
Application note
Application note
2026-06-22
PUBLIC
Tech Note 258: ACS880 min and max torque limits
ID:LVD-EOTKN258U-EN
,
REV:A
English
Some applications require the minimum and maximum torque limits to be adjusted throughout the process. This will discuss a few methods of modifying the torque limits and offer some useful tips.
Application note
Application note
2026-06-22
PUBLIC
Tech Note 255: FEN Encoder Cards emulation cycle time
ID:LVD-EOTKN255U-EN
,
REV:A
English
This document discusses the latency of the emulation signals that are part of the FEN series encoder cards. Below is an example of one of the encoder cards, the FEN-11. The emulation signal we are referring to in this document is the encoder emulation output x43 in the image below.
Application note
Application note
2026-06-22
PUBLIC
Tech Note 254: Parameter restore options for 880, 580, 380 and 180 series drives
ID:LVD-EOTKN254U-EN
,
REV:A
English
This document discusses the parameter restore function and what settings are restored with the different selections in parameter 96.06. Below is an image of the parameter restore from the ACS580 firmware manual.
Application note
Application note
2026-06-22
PUBLIC
Tech Note 253: When is disconnecting varistor screws necessary and why do we need to do it?
ID:LVD-EOTKN253U-EN
,
REV:A
English
Most drive families incorporate a ground-to-phase varistor intended for surge suppression in symmetrically grounded TN-S electrical systems. In networks that do not follow TN-S grounding conventions, the varistor may experience continuous electrical stress beyond its intended operation limits. This Technical Note explains ABB’s requirements for disconnecting the varistor screw in incompatible grounding systems, and why this measure is sometimes necessary.
Application note
Application note
2026-06-22
PUBLIC
Tech Note 251: Assigning IP addresses to 80 series drives
ID:LVD-EOTKN251U-EN
,
REV:A
English
This document discusses how to download and install the ABB IP configuration tool. The document will cover how to assign an IP address to ABB Drives. The ABB IP Configuration tool is part of the Automation Builder installation but can be installed as a standalone tool.
Application note
Application note
2026-04-26
PUBLIC
Tech Note 252: Maximum inrush current when starting a motor
ID:LVD-EOTKN252U-EN
,
REV:A
English
What would be expected with a Variable Speed Drive (VFD)?
Application note
Application note
2026-04-26
PUBLIC
Tech Note 074: Motor heating
ID:LVD-EOTKN074U-EN
,
REV:C
English
This document explains how to enable and adjust the motor pre-heat function in the drive, as well as the advantages of using the VFD pre-heat motor functionality compared to using a traditional motor winding heater.
Application note
Application note
2026-04-08
PUBLIC
Tech Note 248: Energy recovery wheel, variable speed
ID:LVD-EOTKN248U-EN
,
REV:A
English
Energy recovery wheels in AHUs are used to transfer conditioned air energy before being expelled from a building and reuse that energy back into the fresh air being brought in. By recovering this energy, the system overall efficiency is increased. To further reduce energy consumed and provide frost protection, the wheel rotation speed can be varied with a VFD. This technical note details wiring, sensors and programming for an ACH580 drive to control the speed of an energy recovery wheel based off supply and exhaust air temperature sensors.
Application note
Application note
2026-04-02
PUBLIC
Tech Note 249: Network Hand Mode for ACH580 & ACH180
ID:LVD-EOTKN249U-EN
,
REV:A
English
“Hand” mode is a well-established term in the HVACR industry describing an operational state where the normal “Auto” control location, typically hardwired inputs, is overridden at the user control panel to place a drive under local control. Using this familiar term, a similar control mode is introduced called “Network Hand” mode, where this control is taken by the BAS controller to place a drive under network control.
Application note
Application note
2026-04-02
PUBLIC
Tech Note 047: How to setup floating point control
ID:LVD-EOTKN047U-EN
,
REV:B
English
This document describes in detail setup for floating point control/MOP
Application note
Application note
2026-04-09
PUBLIC
Tech Note 250: Redundant communications and control
ID:LVD-EOTKN250U-EN
,
REV:A
English
This technical note is focused on explaining the drive's role within a communications network, understanding the protocol support and configuration to provide redundant protocol communication options, and also briefly introduce how the ACH580 drive can support multiple control modes to utilize the redundant capabilities that are standard features in the ACH580 series drive.
Application note
Application note
2026-04-02
PUBLIC
Tech Note 239: How to test EFB (Embedded Fieldbus)
ID:LVD-EOTKN239U-EN
,
PART:Updated
,
REV:A
English
This document will guide users through the process of wiring and connecting the BCBL-01 RS-485 to USB adapter for the purpose of testing Modbus RTU communication to ABB All Compatible Drives.
Application note
Application note
2026-02-26
PUBLIC
Tech Note 238: ACS880 I/O and Communication Update Times
ID:LVD-EOTKN238U-EN
,
PART:Updated
,
REV:A
English
Process Coordination Reference for ACS880 I/O
Application note
Application note
2026-02-26
PUBLIC
Tech Note 237: Crane/Winch Style Deadband for an Analog Joystick
ID:LVD-EOTKN237U-EN
,
PART:Updated
,
REV:A
English
Document discusses how to use adaptive programming to manage a deadband region in the analog input signal for example a joystick.
Application note
Application note
2026-02-26
PUBLIC
Tech Note 241: Control Panel Compatibility
ID:LVD-EOTKN241U-EN
,
PART:Updated
,
REV:A
English
Which control panel can be used with what drives
Application note
Application note
2026-02-26
PUBLIC
Tech Note 236: EDS File Creation Using Drive Composer Pro
ID:LVD-EOTKN236U-EN
,
PART:Updated
,
REV:A
English
This document will guide users through the process of creating an XML file with Drive Composer Pro and importing it into TwinCAT System Manager.
Application note
Application note
2026-02-26
PUBLIC
Tech Note 246: Design A and B motors with drives
ID:LVD-EOTKN246U-EN
,
REV:A
English
Historically, variable frequency drive specifications have had a requirement for the drive to be able to run a NEMA Design B motor. Whether an HVACR or Water & Wastewater application, this specification item is often glanced over as most motors applied to fan or pump applications have been Design B motors. With the push to increase the efficiency of AC motors, it is becoming more common to see NEMA Design A motors applied to fans and pumps. For example, the ABB / Baldor SP4 induction motor series has IE4 efficiency and uses Design A motors. This technical note discusses the differences between Design A and B motors related to fan and pump applications.
Application note
Application note
2026-01-08
PUBLIC
Tech Note 245: ACH180 retrofit for Nortek AHU with Siemens PLC
ID:LVD-EOTKN245U-EN
,
REV:A
English
The following technical note provides instruction on an ACH180 drive being installed in a Nortek air handling unit that is using a Siemens POL687.0 controller, communicating with the drive using Modbus RTU, reading and writing to the same Modbus addresses and scaled values they previously used with the ACS320.
Application note
Application note
2025-12-31
PUBLIC
Tech Note 244: Basic redundant drive system setup
ID:LVD-EOTKN244U-EN
,
REV:A
English
Some applications require a basic redundant system where a BAS or PLC is not available. For systems with two drives, each connected to a separate motor, some simple control wiring and drive programming can provide a solution without the need for the BAS or PLC to do the controls.
Application note
Application note
2025-12-31
PUBLIC
Tech Note 242: Advanced damper control for E-Clipse bypass
ID:LVD-EOTKN242U-EN
,
REV:A
English
Advanced Damper Control is a feature of the ABB ACH580 to control the sequence of one or two dampers along with starting a fan without external controls required. This technical note details the alternative wiring and programming when an E-Clipse bypass is included with an ACH580 drive. Technical note 52 covers additional details on Advanced Damper Control in an ACH580 drive only.
Application note
Application note
2025-12-31
PUBLIC
Tech Note 017: EC Titanium motor setup with ACH580 and ACH180
ID:LVD-EOTKN017U-EN
,
REV:C
English
This technical note reviews commissioning the EC Titanium motor with ACH580 and ACH180 drives. The EC Titanium motor has embedded magnets which means the drive is programmed differently than with an induction motor. This technical note also includes troubleshooting guidance.
Application note
Application note
2025-12-31
PUBLIC
Tech Note 234: How to read ABB’s drive firmware version
ID:LVD-EOTKN234U-EN
,
PART:Updated
,
REV:A
English
This tech note discusses ways to reconstruct firmware version values transmitted over fieldbus from a non-intuitive data format to a clear decimal representation as it is displayed in drive keypad and Drive Composer software.
Application note
Application note
2025-11-26
PUBLIC
Tech Note 231: Connecting an ABB VFD to a Rockwell PLC
ID:LVD-EOTKN231U-EN
,
PART:Updated
,
REV:A
English
Variable Frequency Drives (VFDs) can be controlled via several methods, one of which is by using a Programable Logic Controller (PLC). This method of control can feature products from different manufacturers, which can sometimes make it difficult for the end user to find the information needed to connect successfully.
Application note
Application note
2025-11-25
PUBLIC
Tech Note 235: Ultra-low harmonic drives
ID:LVD-EOTKN235U-EN
,
REV:B
English
ABB’s low harmonic active front end drives have been known as the Ultra-low harmonic drives for over 20 years. Recently non-ABB manufacturers have started calling their drives “ULH” or “ultra low harmonic,” which has caused confusion in the industry. This technical note provides some history and background information on Ultra-low harmonic ABB drives.
Application note
Application note
2025-11-05
PUBLIC
Tech Note 229: Sustainability and the future of drives and motors
ID:LVD-EOTKN229U-EN
,
REV:A
English
This technical note delves into the future of drives and motors, with a focus on discrete drives and motors and whether they’ll be replaced with solutions like motors that contain integral drives or even ECMs.
Application note
Application note
2025-11-03
PUBLIC
Tech Note 233: China Compulsory Certificate Mark
ID:LVD-EOTKN233U-EN
,
PART:Updated
,
REV:A
English
The China statutory safety certification system and the basic approach to safeguard the consumers' rights and interests and to protect personal property safety.
Application note
Application note
2025-11-26
PUBLIC
Tech Note 232: Writing 32-bit registers using Modbus Poll
ID:LVD-EOTKN232U-EN
,
PART:Updated
,
REV:A
English
This document provides guidance on writing parameters using 32-bit Modbus registers in Modbus Poll, a software tool used to test and simulate Modbus communication as a Modbus master. It helps users ensure that the correct Modbus register addresses are used when communicating with Modbus slave devices—specifically, ABB variable frequency drives (VFDs). This procedure applies to the ABB ACS 380, 580, and 880 VFD models. The compatible fieldbus adapter modules for this method of communication include the FENA-11, FENA-21, and FMBT-21.
Application note
Application note
2025-11-25
PUBLIC
Tech Note 230: Setup of Windows firewall to allow drive connection
ID:LVD-EOTKN230U-EN
,
REV:A
English
The purpose of this document is to ensure successful communication between your PC and the ABB drive using Drive Composer Pro. By properly configuring your computer firewall, you can facilitate seamless communication between Drive Composer Pro and the ABB drive over Ethernet network.
Application note
Application note
2025-11-25
PUBLIC
Tech Note 225: DC Voltage Levels
ID:LVD-EOTKN225U
,
REV:A
English
ACS580, ACQ580 and ACH580 - The following tables show the values of selected DC voltage levels.
Application note
Application note
2025-10-22
PUBLIC
Tech Note 228: BACNet/IP integration to the ACH180
ID:LVD-EOTKN228U-EN
,
REV:A
English
The ACH180 has BACnet MS/TP embedded as standard but this drive is not compatible with the FBIP BACnet/IP option card. This technical note shows how to use a third party router to connect an ACH180 to a BACnet/IP network.
Application note
Application note
2025-10-10
PUBLIC
Tech Note 226: Input current crest factor
ID:LVD-EOTKN226U-EN
,
REV:A
English
Crest factor is a unitless calculation of the “peakiness” that a waveform exhibits and can have negative effects on electrical systems if it exceeds certain limits. Three different ABB drives, the ACH180 microdrive, the ACH580-01 base drive, and the ACH580-31 ULH drive have their crest factor documented in this technical note.
Application note
Application note
2025-10-10
PUBLIC
Tech Note 217: Regenerative and Ultra-low harmonic, line side Autoreset function
ID:LVD-EOTKN217U-EN
,
REV:B
English
Minimize customer drive interaction and eliminate nuisance line side fault resets.
Application note
Application note
2025-07-23
PUBLIC
Tech Note 218: Supervision Controlled Pre-Heat
ID:LVD-EOTKN218U-EN
,
REV:A
English
Use the ambient VFD fan sensor temperature to turn on motor pre-heat function in an ACS880
Application note
Application note
2025-06-23
PUBLIC
Tech Note 221: ACS880 Master Follower Drive to Drive (D2D) Tips and Hints
ID:LVD-EOTKN221U-EN
,
REV:A
English
D2D setup using ACS880
Application note
Application note
2025-06-23
PUBLIC
Tech Note 222: ACS880 Torque control follower with speed window
ID:LVD-EOTKN222U-EN
,
REV:A
English
Speed window control on a torque-controlled follower
Application note
Application note
2025-06-23
PUBLIC
Tech Note 214: Drive Composer Pro allowable IP addresses
ID:LVD-EOTKN214U-EN
,
REV:A
English
IP addresses and classes that can be used to connect to an VFD with Drive Composer Pro
Application note
Application note
2025-06-17
PUBLIC
Tech Note 211: ABB Profile State Machine Work Around
ID:LVD-EOTKN211U-EN
,
REV:A
English
ABB Drives using ABB Profile won’t start after a ramp stop requested
Application note
Application note
2025-06-17
PUBLIC
Tech Note 215: Permanent Magnet Motor ESP Quick Start Guide
ID:LVD-EOTKN215U-EN
,
REV:A
English
Minimum Parameters to Test a PMM ESP Motor using the +N5600 Firmware on an ACS880 VFD
Application note
Application note
2025-06-17
PUBLIC
Tech Note: 216: ACS880 Master Follower Guide
ID:LVD-EOTKN216U-EN
,
REV:A
English
The ACS880 can be used to replace an ACS800 in an existing master follower application without modifying any ACS800 parameters or wiring. As long as the ACS880 is configured properly it can replace an ACS800 as the master or the follower.
Application note
Application note
2025-06-17
PUBLIC
Tech Note 213: Drive Composer not displaying parameter names
ID:LVD-EOTKN213U-EN
,
REV:A
English
After connection with Drive Composer, parameter names are missing
Application note
Application note
2025-06-17
PUBLIC
Tech Note 224: Supply voltage and HVACR drive selection
ID:LVD-EOTKN224U-EN
,
REV:A
English
This technical note focuses on understanding how supply voltage impacts drive selection in an HVACR applications. It reviews a variety of situations, such as when the supply voltage is lower than the motor's nameplate voltage.
Application note
Application note
2025-07-01
PUBLIC
Tech Note 223: Transitioning from CBAI-01 to CAIO-01 with ACx580 Drives
ID:LVD-EOTKN223U-EN
,
REV:A
English
The intention of this document is to address the CBAI-01 transition into the limited lifecycle stage, and the usage of the CAIO-01 as a replacement. It will outline the details on the differences/similarities and identify parameters to be configured.
Application note
Application note
2025-05-26
PUBLIC
Tech Note 220: Power-up Cycle Limits for ABB Drives
ID:LVD-EOTKN220U-EN
,
REV:A
English
To Help in Preventing Pre-charge Circuit Damage
Application note
Application note
2025-06-23
PUBLIC
Tech Note 219: ACS880 Inductance Values
ID:LVD-EOTKN219U-EN
,
REV:A
English
With Percent Impedance by Rating Within a Frame Size
Application note
Application note
2025-06-23
PUBLIC
Tech Note 212: ACS880 Passing a bit over the line side unit comm link
ID:LVD-EOTKN212U-EN
,
REV:A
English
Passing a bit with LSU CW User Bit selection
Application note
Application note
2025-06-17
PUBLIC
Tech Note 207: ULH power factor correction with the 580 series
ID:LVD-EOTKN207U-EN
,
REV:A
English
The ULH 580 series (both ACH580 and ACQ580) have the ability to proactively correct displacement power factor. The extra capacity in a drive can be used for power factor correction. This technical note outlines the power factor correction concept with a drive, along with providing control strategies that can be used.
Application note
Application note
2025-04-16