Data center cooling: Taking uptime, sustainability and energy efficiency to a new level, Brochure
ID:HVAC-PHPB02U-EN
,
REV:A
English
The world depends increasingly on data, computing power and connectivity, making
data centers mission-critical facilities requiring special attention. ABB provides data
centers with reliable, flexible and secure operation. Its solutions ensure continuous
availability while helping to improve performance in a productive and sustainable way.
Heating, ventilation and air conditioning in buildings Enhancing comfort, safety, and energy efficiency in commercial and residential environments, Brochure
ID:HVAC-PHPB01U-EN
,
REV:A
English
Heating, ventilation and air conditioning (HVAC) systems have a significant impact
on both comfort and costs in any building. Modern buildings require smart HVAC systems that create comfortable, healthy and safe environments for the occupants, while minimizing energy consumption and increasing sustainability.
Critical facilities require expertise and solutions to bring you peace of mind. Our redundant drives are always ready for when your system needs them the most.
ABB Drives for HVAC ACH580 E-Clipse Bypass, Brochure
ID:ACH580-PHPB03U-EN
,
REV:A
English
Comfort touches every area of our lives. In every space, there is a high demand to have cool, clean, and comfortable air. The ACH580 E-Clipse Bypass ensures continuous operation for all your critical cooling requirements. Furthermore, our extensive range of bypass options will allow you to customize to your systems, ensuring peace of mind.
Application notes, HVAC - VAV with fan tracking positive pressure - Fact File
ID:AD4
,
PART:1
,
REV:D
English
The idea is to keep the return fan airflow slightly smaller than the supply air flow in order to have a slight over-pressure in the building. FactFile, Fact File
District heating systems play an important role in the efficient and sustainable heating of buildings, since they use less energy than if each building had individual heat generation on site. But it is not enough to generate heat efficiently – it must be transmitted and distributed with minimal cost and energy loss. And ABB has a fleet of cutting edge solutions to support this.
Case notes -ABB standard drives for HVAC improve road tunnel safety - Fact File
ID:CD58
,
REV:A
English
When the E18 road link between Turku and Helsinki in Finland was to be upgraded to a motorway in its entirety, ABB's channel partner Airwecare was called upon to supply, dimension, and install ABB drives to control the tunnel fans. ABB drives are used in the four longest tunnels to manage air flow visibility , fire safety and air quality. Fact File.FactFile
District cooling systems play an important role in the efficient and sustainable cooling of buildings, since they use less energy than if each building had individual cooling generation on site. But it is not enough to generate cooling efficiently – it must be transmitted and distributed with minimal cost and energy loss. And ABB has a fleet of cutting edge solutions to support this.
Although motors date back to the 1880s, work is still being done to improve existing motors and create new designs. The motors
below can be found in commercial HVAC applications. All use a three-phase AC stator which creates a rotating magnetic field that
drives the motor’s rotor. The stator is often powered by a variable frequency drive (VFD).
Data center cooling. Taking uptime, sustainability and energy efficiency to a new level
ID:3AXD50000584352
,
REV:A
English
The world depends increasingly on data, computing power and connectivity, making data centers mission-critical facilities requiring special attention. ABB provides data centers with reliable, flexible and secure operation. Its solutions ensure continuous availability while helping to improve performance in a productive and sustainable way.